Library Import Configuration

Use the
Library Import Configuration
window to define the parameter settings for a library object that is being imported.
The
Library Import Configuration
window has these settings.
Name
Type
Description
01 Library Status
Status
Dropdown menu
If the library is saved as Pending, this revision will be replaced next time changes are saved. If the library is saved as Published, a new revision will be created next time changes are saved.
02 Revision History
Revision Description
Text entry
The revision description of the library object. This is an optional setting.
Reset History
Dropdown menu
Displays different options to keep the current revision history, remove previous revision histories, or clear all revision histories. This is a required setting.
03 Library Details
CatalogNumber
Text entry
The library object name, which appears together with the revision number in the library object listing when the library object is registered in ACM. This is entered manually.
This is a required setting.
Description
Text entry
The description of the library object. This is an optional setting.
Family
Dropdown menu
The Family of the library object. This is a required setting.
Solution
Dropdown menu
The Solution for the library object. This is a required setting.
Library Type
Dropdown menu
The Library Type for the library object. This is a required setting.
Category
Dropdown menu
The Category for the library object. This is a required setting.
Content Type
Text
Displays the type of the object, Task, Program, or Routine.
Owner
Text entry
The user or entity that originally published the library object. This is a required setting.
Major Revision
Text entry (integer)
The major revision number for the library object. For a new library object, this defaults to 1.
If you are updating an existing library a new value will be set based on existing library objects with the same CatalogNumber, unless the library status is Pending.
Minor Revision
Text entry (integer)
The minor revision number for the library object. For a new library object, this defaults to 0.
If you are updating an existing library a new value will be set based on existing library objects with the same CatalogNumber, unless the library status is Pending.
04 Library Usage Rules
Upstream Keys
Text entry
For module library objects: a rule that limits the upstream hardware components that will be made accessible to the library object when it is added to an ACM Project. The rule is entered manually as a logical expression.
Downstream Keys
Text entry
For module library objects: a rule that limits the downstream hardware components that will be made accessible to the library object when it is added to an ACM Project. The rule is entered manually as a logical expression.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal