Add a code item

Add a VBA code item to edit the code in
Library Object Manager
.
Prerequisites
  • Add SE VBA Items to a library object.
To add a common/symbol code item to a library object
  1. Right-click the
    Common Code
    or
    Symbol Code
    subfolder and select
    Add
    , the VBA Code Builder dialog box opens.
  2. Select a display or a class item and click
    OK
    . A common/symbol code item is added to the library object.
    TIP:
    The
    Name Prefix
    substitution in the
    VBA Code Builder
    dialog box will be check by default when adding a symbol code.
  3. Configure the properties as needed.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal