VBA Code Builder

Use the VBA Code Builder to select a common/symbol code to add or update.
Item
Description
Select Display Export File
Select a display export file of VBA items, click the ellipsis (...) button to select another file.
Select Subroutine/s to include
A list of subroutines in the selected file. Select display or class subroutines to add or update.
Select Substitutions to Apply
A list of substitutions in the library, including:
  • Predefined
    A
    Name Prefix
    substitution
  • Saved
    Substitutions saved in the library
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal