Add an item to Custom Collections

Once you apply the changes in
Library Object Manager
, the item you add to
Custom Collections
will display in the
Properties
panel of
Application Code Manager
.
To add an item in Custom Collections
  1. In
    Library Content
    , Right-click
    Custom Collections
    , and then select
    Add
    .
    A folder named
    NewCollection
    is added and you can configure its properties in the Properties panel.
  2. Right-click
    NewCollection
    , and then select
    Add
    .
    An item named
    NewItem
    is added and you can configure its properties in the
    Properties
    panel.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal