Item properties

The following table displays the options in the
Properties
panel of an item object.
Options
Descriptions
Item Name
Displays the name of the item. A condition can be entered manually or generated by an expression. To create an Expression, click the ellipsis (...) button to open the
Expression Builder
.
Include Condition
Displays the Include Condition of the item. The default is
Always
. A condition can be entered manually or generated by an expression. To create an Expression, click the ellipsis (...) button to open the
Expression Builder
.
Add New Attribute
Opens
Attribute Builder
.
Edit Attribute
Opens
Attribute Builder
.
Delete Attributes
Deletes an attribute.
Filter
Enter the key words or the name of an attribute to search it quickly.
Name
Displays the name of an attribute.
Value
Displays the value of an attribute.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal