Add a message to a trigger

Trigger messages describe alarm conditions and properties.
Prerequisites
To add a message to a trigger
  1. In
    Library Repositories
    , select a library object that includes
    FactoryTalk View ME
    Alarms content.
  2. In
    Library Content
    , expand the
    ME Alarms
    folder and select the
    Messages
    subfolder.
  3. Open the Message Builder dialog box with one of the following methods:
    • Right-click
      Messages
      and select
      Add
      .
    • Click Add icon in the Properties column.
    • Right-click in the table of the Properties column and select
      Add
      .
  4. Fill in
    Message Details
    in the
    Message Builder
    dialog box.
  5. Click
    OK
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal