Add a trigger to a library object
FactoryTalk View ME
reads the tag's or expression's value, and generates an alarm when the value matches an alarm message's trigger value.Prerequisites
To add a trigger to a library object
- Right-click theTriggerssubfolder and selectAdd. TheTriggerdialog box opens.
- InTag or Expression, type a tag name or an expression, or click the ellipsis (...) button to choose a tag and clickOK.
- ClickOK.
- Configure the properties as needed.
Provide Feedback