Export an attachment
Export an attachment to an .HZ1 file to transfer it to another database. Exported .HZ1 files are saved with filenames matching their File ID property, such as
8779ddbb-bd37-438c-ab4e-3b6b75051333.hz1
.To export an attachment to an .HZ1 file
- In, select Attachments.Library Object Manager
- Select one or more attachments from the list.
- SelectExport to .HZ1 Attachment Files.
- InBrowse For Folder, select a folder where the file should be exported, then selectOK.
Provide Feedback