Attachments
How do I open Attachments?
- InLibrary Repositories, selectAttachments.
Use
Attachments
to add, edit, remove, import, or export file attachments to or from an Application Code Manager
database.Button or Column | Description |
|---|---|
Add New Attachment | Opens Attachment to add an attachment file to the database. |
Edit | Opens Attachment to edit the properties of an existing attachment file. |
Delete Attachments | Removes the selected attachment files from the database. |
Extract Files | Extracts the selected attachment files to a folder location. The output files are
extracted to their original filenames and formats. |
Export to .HZ1 Attachment Files | Exports the selected attachment files to a folder location. The output files are
exported with filenames matching the file ID in the .HZ1 format. |
Import from .HZ1 Attachment Files | Imports one or more .HZ1 format attachment files from a folder location. |
Filter | Limits the attachment list to attachments with properties matching the characters entered in the Filter field.The filter function uses exact character matching and is case insensitive. Wildcard characters are not supported. |
Select | Toggles whether a row is selected before deleting or exporting the attachments. |
Name | Displays the name of the attachment. |
Description | Displays the description of the attachment. |
File Name | Displays the original file name of the attachment. |
File ID | Displays the unique file identification number of the attachment. |
Revision Description | Displays the latest revision description of the attachment. |
Modified Date | Displays the last modified date of the attachment. |
Modified By | Displays the last user that modified the attachment. |
Provide Feedback