Edit an attachment

Edit an attachment in an
Application Code Manager
database to change the properties of an attachment. Editing an attachment does not modify its unique File ID.
IMPORTANT:
Editing an attachment in an
Application Code Manager
database updates the attachment every library that references it.
To edit an attachment
  1. In
    Library Object Manager
    , select
    Attachments
    .
  2. Select the attachment from the list.
  3. Click
    Edit
    .
  4. In Attachment, change the properties of the attachment, then click
    OK
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal