Attachment
How do I open Attachment?
Either:
- InAttachments, selectAdd New Attachment.
- InAttachments, select an existing attachment, then selectEdit.
Use
Attachment
to set or edit the properties of an attachment.Field | Description |
|---|---|
File ID | Displays the unique file identifier of the attachment. |
Name | Sets the name of the attachment. |
File | Sets the filename of or path to the attached file. |
Description | Sets the description of the attachment. |
Revision Description | Sets the description of the last change or revision to the attachment. |
Last Updated | Displays the last date and time that the attachment was revised. |
Last User Updating File | Displays the last user that revised the attachment. |
Provide Feedback