Add an attachment

Add an attachment to an
Application Code Manager
database before referencing and publishing them using a library.
To add an attachment
  1. In
    Library Object Manager
    , select
    Attachments
    .
  2. Click
    Add New Attachment
    .
  3. In Attachment, enter a name and description for the attachment.
  4. In
    File
    , enter a path or click the ellipsis button
    (...)
    to browse for a path to a file.
  5. (optional) In
    Revision Description
    , enter a revision message describing the changes to this attachment for this revision.
  6. Click
    OK
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal