Using the component browser
You can use the component browser to specify components for particular graphic objects. The only objects that this currently applies to are the Local Message Display and Display List Selector.
To use the component browser:
- InFactoryTalk View Studio, on the graphic display, select an object.
- In theProperty Panel, in thePropertiestab, click the property that takes a component.TIP:The property isMessageFilefor the Local Message Display, andDisplayorParameterfor the Display List Selector.
- Click the browse button (...) beside the property.
- In theComponent Browser, select one of the property's components. It is called when the object is activated at runtime.
Provide Feedback