Tab index

Type a number to specify the order in which the Tab key will select the button. If you leave this blank, the Graphics editor assigns the next index number available for the display. If you specify a number, the existing index numbers are adjusted to accommodate it.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal