Static objects
A static object does not initiate actions or change to reflect current processes or tag values. It is used for illustrative purposes. However, you can attach animation to static objects (except the image and panel objects) if you want the object to act as an indicator of a changing tag value.
The drawing objects and the scale object are static objects. Objects that are converted to wallpaper are also static, and animation does not affect them.
Provide Feedback