Time Date Display Properties - General tab
The following table shows options under
Appearance
of the General
tab.Options | Description |
|---|---|
Border style | Select the border style. If the object is a circle or ellipse, the available border styles are None and Line. |
Border width | Type the number of pixels for the width of the object’s border. |
Back style | Select whether the object background is solid, gradient, or transparent. If you select Transparent, the object’s background is not filled in and any objects behind it show through. If you select Gradient, the object's background is filled with a linear gradient color. |
Pattern style | Select a pattern for the object. The pattern appears on the face of the object. The pattern does not cover the object’s border, caption, or image (if any are defined for the object). If the object’s back style is transparent or gradient, the pattern is not visible. |
Border uses back color | Select this check box to use the object’s background color for the border of the button. If this is not selected, you can assign a separate color to the border, instead of using the object’s background color. |
Back color | This field displays the current background color for the object or state. Click it to select another color. If the background style is transparent, the application does not use this background color. If the background style is gradient, click it to bring up the gradient fill dialog box to configure the gradient fill. For objects with a line style other than Solid, the background color is used for the spaces between the dots or dashes. |
Border color | This field displays the border color for the object or state. Click it to select another color. If Border uses back color, is not selected, this color appears at runtime. |
Pattern color | This field displays the current pattern color for the object or state. Click it to select another color. |
Fore color | This field displays the current color for the object’s text or line. Click it to select another color. |
Blink | Select this check box if the object’s background is to blink at runtime. The blink rate is twice per second. If you select a pattern style, the pattern also blinks. |
The following table shows options under
Text
of the General
tab.Options | Description |
|---|---|
Text | The text properties apply to the time and date text in the display. |
Font | Select the font to use for the caption or message. |
Size | Select the font size to use for the caption or message. |
Bold (B), Italic (I), Underline (U) | Click a letter, or letters, to specify the font style for the caption, if required. |
Word wrap | Check this box if the caption or message is to continue on the next line at the beginning of a new word. If this is not checked, the caption or message continues on the next line whenever the maximum text length is reached, even if this occurs in the middle of a word. The maximum text length depends on the width of the object and the font size. |
Alignment | Click a button to specify how the text is to be positioned on the object. |
The following table shows options under
Time and date format
of the General
tab.Options | Description |
|---|---|
Time and date format | Select the time and date format to display. The available options reflect the settings in the development computer’s operating system. If the operating system settings are different on the development and runtime systems, the runtime settings are used at runtime. In the Property Panel, the name of this property is Format. |
Provide Feedback