Symbol Properties - General tab

The following table shows the options under
Appearance
in the
General
tab.
Table Heading
Table Heading
Border style
Select the border style. If the object shape is circle or ellipse, the available border styles are None and Line.
Border width
Type the number of pixels for the width of the object’s border.
Shape
Select the shape of the object. If the object shape is circle or ellipse, the application applies properties such as size and position by measuring in relation to the object’s bounding box.
The following table shows the options under
Symbol settings
in the
General
tab.
Table Heading
Table Heading
Number of states
Select the number of states for the object.
Trigger type
Choose Value to trigger a state based on the value of the Indicator connection.
Choose LSB if the object is to trigger a state based on the least significant bit that is set high in the Indicator connection.
Image
Select the file name of the graphic image for the object or state. The image appears on the face of the object, to give the operator information about what the object does or about the current state. Before you can place an image on the object, you must import the image into your project.
You must use a monochrome image with this object.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal