Set up how the symbol indicator looks

Use the
General
tab to set up how the symbol indicator looks. After you set up the options in the General tab, click the
States
tab to specify how the indicator looks in each state at runtime.
To set up general options for the symbol indicator:
  1. In a display, double-click the object to open the
    Symbol Properties
    dialog box.
  2. Click the
    General
    tab.
  3. Specify these properties:
    • general appearance
    • symbol settings
      TIP:
      Before you can select an image for the indicator, you must import the image into your project.
      If the image is not a monochrome bitmap, or if the bitmap has been removed from the project, an X appears on the indicator.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal