Set up a connection for a multistate indicator
Use the
Connections
tab to set up a connection for a multistate indicator object.To set up a connection for a multistate indicator
- In a display, double-click the object to open theMultistate Indicator Propertiesdialog box.
- Click theConnectionstab.
- Assign a tag or expression to the Indicator connection.Indicator is read connection. If you assign a tag, the application reads the value at the data source, assigns this value to the Indicator tag, and updates the object in the display to reflect the state corresponding to the value or least significant bit value, depending on the trigger type.If you assign an expression, the application calculates the value of the expression and updates the object's display to reflect the corresponding state or least significant bit value, depending on the trigger type.
Provide Feedback