Configure general properties of a multistate indicator
fter you set up the options in the
General
tab, click the States
tab to specify how the indicator looks in each state at runtime.To configure general properties of a multistate indicator:
- In theMultistate Indicator Propertiesdialog box, in theGeneraltab, specify the following properties if needed:
- general appearance
- number of states and trigger type
Provide Feedback