Set up values and thresholds for a gauge
Use the
Display
tab to set up values and thresholds.To set up values and thresholds for a gauge:
- In a display, double-click the object to open theGauge Propertiesdialog box.
- Click theDisplaytab.
- Specify these properties:
- minimum and maximum values
- legends, if any
- thresholds, if any
Provide Feedback