Gauge Properties - Display tab
The following table shows options under
Value settings
.Options | Description |
|---|---|
Minimum value | Type the lowest value for the gauge. If the Value connection is at or below this value, the needle is at the left end of the dial. |
Maximum value | Type the highest value for the gauge. If the Value connection is at or above this value, the needle is at the right end of the dial. |
Legends are captions beside each major tick mark. The caption corresponds to the value at the part of the dial where the tick mark is located. The following table shows options under
Legend settings
.Options | Description |
|---|---|
Show legend | Select this check box if you intend to include legends on the gauge object. |
Digits after decimal | Select the number of digits to show after the decimal point. |
Legend color | This field displays the current legend color. Click it to select another color. |
The following table shows options under
Thresholds
.Options | Description |
|---|---|
Number of thresholds | Select the number of thresholds for the object. Select 0 if you do not want to use thresholds. |
Threshold type | Select whether to use an absolute value, or a percentage of the range between the minimum and maximum values, for the thresholds. |
Threshold 1 value | Type the value or percentage for the first threshold. |
Fill color | This field displays the current fill color for the section of the dial that’s at or above the first threshold and below the second threshold (if enabled). Click it to select another color. If the sweep style is gradient, click it to bring up the gradient fill dialog box to configure the gradient fill. This color is not used if you select point for the sweep style (on the General tab). |
Blink | Select this check box if the section of the dial that’s at or above the first threshold (and below the second threshold, if enabled) is to blink at runtime. The section of the dial blinks twice per second. |
Threshold 2 value | Type the value or percentage for the second threshold. |
Fill color | This field displays the current fill color for the section of the dial that’s at or above the second threshold. Click it to select another color. If the sweep style is gradient, click it to bring up the gradient fill dialog box to configure the gradient fill. This color is not used if you select point for the sweep style (on the General tab). |
Blink | Select this check box if the section of the dial that’s at or above the second threshold is to blink at runtime. The section of the dial blinks twice per second. |
Provide Feedback