Create a display list selector
Use the display list selector to show a list of graphic displays that the operator open at runtime. The operator can scroll through the list and select a graphic display.
The operator can use the arrow keys on the keyboard to scroll through the list, and press Enter to open a display. You can also create and set up key buttons on the display to provide the same functions.
TIP:
For network distributed applications, display list selectors work with graphic displays located in the home area only.
To create a display list selector:
- InFactoryTalk View Studio, in theGraphicseditor, selectObjects>Advanced>Display List Selector. You can also click the display list selector icon in the toolbox.
- Drag the mouse to position and draw a rectangle the general size and location you intend the display list selector to be.
- In theDisplay List Selector Propertiesdialog box, in the tabs, specify how the selector looks and set up a state for each display the operator can open from the display list selector object at runtime.
Provide Feedback