- Getting started
- Creating projects
- Graphic objects
- Predefined graphic objects
- Object and variable references
- Extending projects
- Tutorials
- Graphic objects tutorial
- NetLogic tutorial
- OPC UA tutorial
CODESYS Tag
Properties
Name | BrowseName | DataType | Description |
---|---|---|---|
Symbol name | SymbolName | Tag name | |
Maximum length | MaximumLength | (string data only) Maximum number of characters in the string | |
Encoding | Encoding | Decode of memory location contents mode | |
Start array index | StartArrayIndex | ||
Array update mode | ArrayUpdateMode | (Inherited from Tag) | |
Original data type | OriginalDataType | (Inherited from Tag) |
Provide Feedback