Discover new Historian points
Use the
Discover New Historian Points
dialog to specify the point source and scan rate for the point discovery process. Historian points can be collected from Logix controllers (for example, ControlLogix), programmable logic controllers (for example, SLC 500), other OPC servers (for example, KEPServer Enterprise), and HMI servers (for example, FactoryTalk View
).To discover new Historian points
- In the Explorer window of theFactoryTalk Administration Console, right-click theFactoryTalkapplication from which you want to collect points, and then selectDiscover Historian Points.
- In theDiscover New Historian Pointsdialog, configure the following:SettingDescriptionHistorian serverSelect the appropriateFactoryTalk Historian SEserver to which you want to add points.Data collection interfaceSelect the appropriate interface for data collection.Search fromSelectBrowseand select the application from which you want to collect points.Add points from these sourcesSelect the point sources that you want to search for, including:
- FactoryTalk Linx
- RSLinx Classic
- HMI/Alarm Servers
- OPC-UA Servers
- Other OPC-DA Servers
Activated discovery ruleSelectDiscovery rulesand select the rule file that you want to use for discovering Historian points.TIP:For more information on the Discovery Rule Editor, select the Help icon in the dialog.Enable data type filterUse this checkbox to filter data type.- If it is selected, auto-discovery will get all attributes that match the name, user-defined tag (UDT), and data type rule.
- If it is cleared, auto-discovery will ignore the data type filter and only check the name and UDT rule.
Default scan rateSelect the time interval at which points will be collected. - SelectDiscover tags.The tags are added to the right pane of theDiscover New Historian Pointsdialog.
- (optional) Double-click the scan rate for each point to change the scan rate value.
- SelectAdd Pointsto add the individual Historian points by configuring the following, and then selectBrowse tags.
- From application: Select the application from which you want to collect points.
- Tag attributes for new points: Select the tag attribute file from which you assign the tag attributes to the new points.
- SelectDeleteto remove the selected Historian points.
- SelectExport Pointsto export the selected Historian points to a CSV file. The default path isC:\ProgramData\Rockwell Automation\FactoryTalk Historian. Edit the attributes of Historian points as needed, and then use PI Builder to import the Historian points into theFactoryTalk Historianserver.TIP:You must install PI Builder first to use its features.
- Select the checkboxes next to the Historian points that you want to add to theFactoryTalk Historian SEserver, and then selectConfirm points.
indicates that the Historian point has been added to the FactoryTalk Historian SEserver successfully.
indicates that the Historian point failed to be added to the FactoryTalk Historian SEserver. Hover over this error icon to see the error messages.
- SelectCloseto return to theFactoryTalk Administration Console.
Provide Feedback