Install PI Builder
Use PI Builder to import and export data points (tags) in the
FactoryTalk Historian
server.To install PI Builder
- Install Microsoft Excel.
- In theFactoryTalk Historian SEinstallation package,go to theRedist\PIAFClientfolder, and then double-clickAFClient_x64.exe.
- UnderApplication Maintenance, selectNext.
- UnderSelect Features, expandPI Builder, selectWill be installed on local hard drive, and then selectNext.
- In thePI AF Client 2024 Setup dialog, selectResume.
- SelectNext.
- UnderReady to Modify the Application, selectInstall.After the installation, thePI Buildertab shows on the Ribbon in Microsoft Excel.TIP:If thePI Buildertab does not show, do the following:
- In Microsoft Excel, go toFile>Options>Add-ins.
- At the bottom of theExcel Optionswindow, selectCOM Add-insfrom theManagelist, and then selectGo.
- In theCOM Add-insdialog, selectPIAFBuilder, and then selectOK.
Provide Feedback