Application Notes

These application notes apply to
FactoryTalk® Edge Gateway
distributed version 1.00.00.
For best results, observe these data flow limits for data sources and destination systems:
Description
Limit
Notes
SQL Server®
10000 tags@ 1000 ms
-
Azure® IoT Hub
1000 tags @ 1000 ms
Depends on the application that uses
Azure IoT Hub
as a transport and system configuration (for example, Event Hub)
InfluxDB
10000 tags @ 1000ms
-
Device and drives limits
Description
Limit
Notes
Drives and IMC devices
Minimum spacing between messages to a drive is 100 ms
Example: If reading 20 parameters, it would take a minimum of 2s to read the parameters
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal