System Requirements

FactoryTalk® Edge Gateway™ works within the system requirements of all Rockwell Automation® software products.
Hardware requirements
FactoryTalk Edge Gateway requires hardware that meets or exceeds these specifications:
  • 8 GB of memory
  • Dual-core processor
Rockwell Automation recommends at least 32 GB of available drive space for FactoryTalk Edge Gateway.
TIP:
The hardware footprint affects application sizing. For more information, see
Data flow limits
in Application Notes.
Software requirements
FactoryTalk Edge Gateway requires the following software on the host computer:
  • Operating system
    FactoryTalk Edge Gateway runs on the following Windows® operating systems:
    • Windows 11 Professional or Enterprise edition (64-bit)
    • Windows 10 Professional or Enterprise edition (64-bit)
    • Windows 10 IoT Enterprise 2016
    • Windows Server 2022 Standard
    • Windows Server 2016 Standard
    • Windows Server® 2012 R2 Standard
When you install FactoryTalk Edge Gateway version 1.04.00, the following softwares will be installed if not already present:
  • Microsoft .NET Framework version 4.8
  • Microsoft ODBC Driver 18.0 for SQL Server x64 version 18.0.1.1
  • OPC .NET API version 2.01.10600
  • FactroryTalk Diagnostics version 6.31
  • Windows Firewall Configuration Utility version 1.00.16
  • CodeMeter Runtime Kit version 7.51.5429
  • Electronic Data Sheets Reader version 35.0.13
  • FactoryTalk Services Platform version 6.31.00
  • FactoryTalk Activation Manager version 5.00.12
  • EtherNet IP Address Commissioning Tool version 2.01.00
  • FactoryTalk Updater Agent version 4.00.00
  • Rockwell Automation x64 Driver version 2.03.06
FactoryTalk Edge Gateway
and
Studio 5000 Smart Object Configurator
compatibility
FactoryTalk Edge Gateway
version
Studio 5000 Smart Object Configurator
version
1.00.00
1.0
1.01.00
1.1
1.01.01
2.0
1.02.00
2.0
1.03.00
2.01.00
1.04.00
2.02.00
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal