System Features

FactoryTalk Edge Gateway
version 1.04.00 introduces these features:
  • Device Discovery tag selection - possibility to select exactly which tags of device profile should be used in the model.
  • Intelligent devices 'Symbolic Tags' reading support.
  • Extended FactoryTalk Live Data adapter possibilities and adoption to work on remote machines using new FT Live Data Remote Connector.
  • Improved performance of namespace operations (population/deletion/clearing).
  • Improved deploy performance of PTC ThingWorx application.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal