Anomalies Corrected in this Release
The list identifies the anomalies corrected in
FactoryTalk Edge Gateway
version 1.04.00. Use the identification information provided in the anomaly heading to track the anomaly in future releases or for reference when receiving assistance from customer support with a related issue.User-defined data types and arrays take longer to populate when using FactoryTalk Live Data shortcut (950637)
Configuring a data source by using FactoryTalk Live Data shortcut causes controllers with user-defined data types and arrays to take longer to populate.
FactoryTalk Live Data shortcuts OPC DA servers do not appear in the data source browse list (1061171)
FactoryTalk Live Data shortcuts to OPC DA servers do not appear in the data source browse list and do not allow proper data egress to applications.
Validation errors occur during import when model and node names contain periods (1270844)
Adding a period in the name of a model or node causes validation errors during import.
Window unresponsive when opening large models (1289774)
Large models might cause the Export window to become unresponsive for some time.
After upgrading FTEG from version 1.02 to 1.04 or 1.03 to 1.04, it is not possible to assign activations (1786569)
There is some issue with the FTAM version 4.06 when used with FTEG version 1.04.00. It is recommended not to use FTAM version 4.06 with FTEG Version 1.04.00.
Unable to add an application when datasource is in the "Loading" status (1580791)
It is impossible to add an application, when a data source is in the Loading state. User will get empty list of applications.
Unable to add a new data source when the previous one in the `Loading` status (1544853)
Adding a new data source when the previous one is in the "Loading" state,will result in not being added to the list.
Missing tags when using FTLD driver to populate data source with OPC DA server pointed to RSLinx OPC server topic (1314466)
Using FTLD driver to populate data source with OPC DA Server pointed to RSLinx OPC server topic can result in some tags missing.
Lost synchronization between FTEG and FTEG-CT after an hour of user inactivity (1746627)
After an hour of user inactivity FTEG-ct stop synchronizing with FTEG service. For example, you can select to go online/offline, but after that the application does not change its status. It is possible to configure a new driver, however after saving the changes the driver does not display at all. Device discovery Profile list does not appear for new Data Source. There is also no information in the FTEG service about adding an adapter for the driver or regarding the data source.
Missing generic CIP tags in PF523/525/753/755 (1635388)
In DD profiles of drives PF523/525/753/755 missing CIP generic tags."$extend": "family.cip.json" - missing fragment of code in each of these profiles.
Can not delete driver (2085966)
You cannot delete a driver if it was previously used with data source which was deleted already and not exist on UI.
AOP tags with BAD quality (1924919)
User should see AOP (Add-On Profiles) tags values in FactoryTalk Edge Gateway.Using CIP driver, user can see only tag names, and time stamps but value quality is 4.
When port 44818 is occupied by other application DD data source stuck in Loading status (1656961)
When port 44818 is occupied by other application, broadcast cannot be done. FTEG tries to populate and waits in “loading” state. Because of this, next datasources which user tries to add waits in line (are queued) also in status “loading” until first datasource will be populated.Status of datasource should be changed to Not populated after timeout and this datasoucre should not block rest of datasources.
FTLD adapter can't be used with FT Linx Gateway OPC UA Server (1988773)
Datasource reading tags from FTLinx Gateway OPC UA Server can't be populated.
FTLD/OPCUA Connector - All tags configured in the Local Directory are not collected (2040543)
FTLD/OPCUA Connector - All tags configured in the Local Directory are not collected. Tags configured in the Network directory work properly.
FTLD/OPCUA Connector - String and Array tags are not collected (2040520)
Strings and Arrays are not collected when using FTLD\OPCUA Connector. Quality of tags is “0” value is “false”.
None of the data types work thru FTLD to SLC 500 (1334332)
FT Live Data is able to get the data, but FTEG is not...comes back with quality 0 using FTLD Driver thru FTLInx to a SLC 500.
See also
Provide Feedback