Connect FactoryTalk Design Studio to FactoryTalk Remote Access
FactoryTalk Design Studio
uses a custom FactoryTalk Remote Access
user named
FTDS
to communicate to on-premises devices through FactoryTalk Remote Access
endpoints. To confirm this user’s configuration, see Enable FactoryTalk Remote Access for FactoryTalk Design Studio. Access to the Build and
Deploy Center requires the Engineer role. To change communication configuration, a FactoryTalk Design Studio
Core entitlement is required.Connect
FactoryTalk Design Studio
to FactoryTalk Remote Access
once the FactoryTalk Remote Access
configuration is complete.- On the top toolbar, select
to open
Deploy center.TIP: You can also selectDeploy centerat the bottom of theDevicesexplorer. - OnDeploy center, in thePathcolumn, select
,
and then select Set controller path.The list of drivers on this screen is common to all users and allFactoryTalk Design Studioprojects in yourFactoryTalk Huborganization. - InSet device path, select
.TheConfigure Driversdialog appears. - InConfigure Drivers, do the following:
- InAvailable Driver Types, selectFactoryTalk Remote Access (VPN).
- SelectAdd New.
TheChange the VPN Endpointdialog appears and shows theFactoryTalk Remote Accessendpoints that haveFTDSuser permissions assigned to them. - InChange the VPN Endpoint, select theFactoryTalk Remote Accessendpoint or device to which you want to connect, and then selectOK. The on-premises controller must have a network connection to this endpoint to be visible toFactoryTalk Design Studio.
- InConfigure VPN, do one of the following:
- SetDiscovery MethodtoDevice List/Range, and then add a specific IP address or range of IP addresses in theDevice List/Rangefield.
- SetDiscovery MethodtoBroadcast. Broadcast discovery finds all available controllers connected to the selected endpoint.
- SelectOKto add your new endpoint.
- SelectClose.Your new endpoint appears in theSet device pathlist and is available to all projects within your organization.
- Right-click the endpoint, and then selectConnect.An active connection to theFactoryTalk Remote AccessVPN endpoint is established and a list of all available controllers connected to that endpoint appears.
- Once connected, expand the list to see available controllers.
- Highlight the controller whose path you want to set, and then selectOK.
FactoryTalk Design Studio
is configured to communicate through your FactoryTalk Remote Access
endpoint, and you’ve set your on-premises controller path.Provide Feedback