Deploy to a physical controller or an on-premises emulated controller
- Set the physical controller's key switch or toggle switch to REM (Remote). If the mode switch on the physical controller is set to RUN, you cannot deploy a project to it fromFactoryTalk Design Studio.
- On the top toolbar, select
to open
Deploy center.TIP: You can also selectDeploy centerat the bottom of theDevicesexplorer. - OnDeploy center, set the device path for each controller.TIP: You can type a path or select the path through the driver in theFactoryTalk Linxbrowser component. To open theFactoryTalk Linxbrowser, in thePathcolumn, select
, and then select Set controller path. To add a VPN driver, see Add a VPN driver. - Select the checkboxes for the controllers to which you want to deploy the project.TIP: Before deploying to a 5069CompactLogixcontroller, verify that theEtherNet/IP™port configuration in the project matches the target device.
- SelectDeploy.
- InDeployment warning, selectContinue.A progress bar indicates the status of the current build and deployment for the controller.
- InChoose a controller to go online with after deployment ends, select a controller, and then selectOK.TIP: You can be online with only one controller at a time. If you are currently online with a controller and choose to go online with a different controller, you automatically go offline with the current controller, and all monitoring tabs are closed.
Provide Feedback