Use instruction-based equipment modules
Equipment modules that derive from a material-based recipe (MBR) phase can be instruction-based or automation-based. When you are working with an instruction-based equipment module, the phase parameters show up as part of the instructions, and phase reports consist of data from the instructions. The MBR generates a prompt, which is formatted into instructions by the Server.
e
Procedure
\t\t\t
Sample of an MBR-generated prompt
TIP:
If there is more than one parameter prompt for any
given control step, each prompt is displayed in a separate instruction step row.
The MBR function uses a number of parameters and reports. The table below describes how they are used within the instruction files:
e
ProcedureName | Parameter/ Report | Used in an Instruction... |
|---|---|---|
AMOUNT | Parameter | As data to be viewed by the operator |
MATERIAL | Parameter | As data to be viewed by the operator |
LOT | Parameter (optional) | As data to be viewed by the operator (might be necessary for the operator to locate the specific quantity) |
LABEL | Parameter (optional) | As data to be viewed by the operator (might be necessary for the operator to locate the specific quantity) |
CONTAINER | Parameter (optional) | As data to be viewed by the operator (might be necessary for the operator to locate the specific quantity) |
ACTUAL_AMOUNT* | Report | Entered by the operator |
FEED_COMPLETE* | Report | Defaults to TRUE to indicate that the feed and phase completed successfully. |
If the prompt in question has a pending signature request, the submit button is replaced with the words "Prompt Pending Signature".

You can acknowledge the signature by clicking the
Signatures
button in the View Selection area to open the Signature List view. Double-click the appropriate signature to display the Signature Request for the prompt. Complete the Signature
dialog box, click Sign
, and then click Close
, and return to the Instructions view to continue. (See the Use the Signature list view
topic for more information.)Provide Feedback