Help button
The Client and the ActiveX Controls, depending on the current Client focus, as described below:
Help
button accesses user assistance for the e
Proceduree
Proceduree
ProcedureHelp
button in the View Selection area to open the user assistance file for the e
ProcedureActiveX Help:
Press the F1
key while an ActiveX control has focus to open the user assistance file for the e
Procedure
TIP:
If selecting
Help
from the Microsoft Internet
Explorer menu bar or pressing F1
when an ActiveX control does not have focus, the
user assistance for Internet Explorer opens.Provide Feedback