PromptsList control
The
PromptsList
control displays a list of prompts and instructions
waiting to be acknowledged and a list of electronic signatures associated with a batch that
are waiting for signoff. Prompts alert operators to requests for information. A control recipe cannot complete execution until the operator provides the requested information. A pending request for information remains unacknowledged until a user provides the information, stops, or aborts the control recipe. Requests for information include prompts, manual instructions, and signatures.
- Prompts alert operators to requests for parameter values, unit binding, and material binding.
- Instructions are individual steps of a manual instruction phase. As a batch executes, the instruction or set of instructions for each active step appears. Instructions execute in the order specified within the master recipe.
- Signatures are requests for signoffs that require user permissions and optional comments. When a signature is generated against a control recipe, acknowledge the signature by completing the associated signoffs. The requested user information in a signature is determined by the signature template.
Refer to the to learn more about:
- PromptsList control methods
- PromptsList control properties
- PromptsList control events
- PromptsList control scripting support
- Base filter shortcuts for the PromptsList control
Provide Feedback