FactoryTalk Batch View HMI Controls

The
FactoryTalk® Batch View HMI Controls
interface allows users to monitor and interact with the production process within a
FactoryTalk® View Site Edition (SE)
Display Client. The
FactoryTalk Batch View HMI Controls
consist of:
  • BatchesList control:
    Creates control recipes, is shown as current control recipes, and commands a control recipe. In
    FactoryTalk View SE
    , the
    BatchesList
    control maps to
    BatchViewHMI.BatchesList
    in the
    Insert an ActiveX Control
    dialog and the
    Property Panel
    .
  • PromptsList control:
    Shows a list of prompts that are waiting to be acknowledged; a list of electronic signatures associated with a batch, which are waiting for signoff; and instructions waiting to be acknowledged. In
    FactoryTalk View SE
    , the
    PromptsList
    control maps to
    BatchViewHMI.PromptsList
    in the
    Insert an ActiveX Control
    dialog and the
    Property Panel
    .
  • SFC control:
    Enables the ability to command batches during
    FactoryTalk View SE
    run-time on the
    Details
    and
    Summary
    pages of the SFC. In
    FactoryTalk View SE
    , the
    SFC
    control maps to
    BatchViewHMI.SFC
    in the
    Insert an ActiveX Control
    dialog and the
    Property Panel
    .
  • Full control:
    Accesses the entire
    FactoryTalk Batch View
    site. In
    FactoryTalk View SE
    , the
    Full
    control maps to
    BatchViewHMI.FullView
    in the
    Insert an ActiveX Control
    dialog and the
    Property Panel
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal