View synchronization issues
Under certain circumstances, a
FactoryTalk Batch
phase or a Logix Designer
equipment phase cannot be synchronized. When this occurs, the Synchronize with Logix5000:<data server name>
dialog box displays a Resolution
of Cannot Synchronize
. To view synchronization issues:
- Select the phase that cannot be synchronized.
- SelectDetailsto see a message that explains why the phase cannot be synchronized. For a list of messages, seeCannot Synchronize messages - create or update area model.
Provide Feedback