Cannot Synchronize-create or update
This table lists the
Cannot Synchronize
messages in the Equipment Phase Synchronization Details
dialog box for equipment phases that exist in Logix Designer
:Message | Description | How To Resolve |
|---|---|---|
The configuration of this Logix Designer - only equipment phase contains values that can only be defined by FactoryTalk Batch Equipment Editor . | The equipment phase was originally created in the project file by synchronizing a FactoryTalk Batch phase that was configured with control strategies, material-based functionality, or limit tags. The corresponding FactoryTalk Batch phase class no longer exists in the area model. | Recreate the Phase Class in the area model with matching configuration and tags. Match the Phase Class name to the Recipe Phase name. Tip: See the Details of the Logix Equipment Phase for the recipe phase and parameter names.Then synchronize again, selecting the Create in Area Model Resolution. |
Provide Feedback