Upload lot attributes

Configure the PXRQ instruction in
Logix Designer
to upload one attribute of a lot from a specified report ID. The attribute identified by the attribute ID uploads from the specified tag into the database if security and write-protections allow. Only one value may be uploaded at a time.
PXRQ instruction configuration
External Request
Data Value Array Element
Value
Upload
Material Manager
Database Data
DINT[0]
6
DINT[1]
Report ID lot data uploads from.
DINT[2]
Lot Controller ID
DINT[3]
Attribute ID
TIP:
The data type in the controller must match the data type of the report ID specified in the data value array element DINT[1].
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal