Material database requests

Use the PXRQ instruction in the phase logic to request material data within the material database. These requests provide a means for accessing or storing a value to or from the material database. This provides the greatest flexibility for customization of phase logic and use of the database.
TIP:
The data type in the controller must match the data type of the parameter or report ID specified in the data value array element DINT[1].
This is a summary of the material database requests:
Summary of the material database requests
External Request
DINT[0]
DINT[1]
DINT[2]
DINT[3]
DINT[4]
Description
Download Material Database Data
0
Parameter ID
Controller ID
Attribute ID
Download Material Attributes
Download Material Database Data
1
Parameter ID
Controller ID
Attribute ID
Download Lot Attributes
Download Material Database Data
3
Parameter ID
Controller ID
Attribute ID
Download Container Attributes
Download Material Database Data
4
Parameter ID
Material ID
Container ID
Feed Type:
1-Addition
2-Distribution
Downloading Container Priority Assignments
Download Material Database Data
5
Report ID
Controller ID
Attribute ID
Uploading Material Attributes
Download Material Database Data
6
Report ID
Controller ID
Attribute ID
Uploading Lot Attributes
Download Material Database Data
8
Report ID
Controller ID
Attribute ID
Uploading Container Attributes
Upload Material Database Data
9
Report ID
Material ID
Container ID
Uploading Container Priority Assignments
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal