Use automatic restart control to restart the FactoryTalk Batch Server services

Learn how to use automatic Windows Service restart control to restart the
FactoryTalk® Batch
Server services after a failure.
The
FactoryTalk Batch
Server maintains a detailed record of every recipe’s state as the recipe is running. If the
FactoryTalk Batch
Server computer were to lose power or otherwise fail, use the automatic Windows Service restart control feature to restart the server on a failed server node. This is enabled by default during a
FactoryTalk Batch
Server installation.
Upon automatic restart of the server in a non-Cold restart, the following functions are placed into the state that existed before termination of the server:
  • Control Recipes
  • Semi-Auto Phase Control
  • Arbitration
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal