FactoryTalk Batch Server Windows service configuration
FactoryTalk Batch
Server configuration can be verified and customized as needed. Configuration includes
specifying the startup type (Automatic or Manual), and setting the server options.
TIP:
The
FactoryTalk Batch
Server service is configured to run as a Windows domain user. Changing the user account
in which the server runs is done through Services.Provide Feedback