Modify FactoryTalk Batch Equipment Editor configuration options
Modify the configuration options in product policies created in the
FactoryTalk
Local Directory for the editors. The following example is specific to
FactoryTalk Batch Equipment Editor
. FactoryTalk Batch Recipe Editor
configuration options are configured similarly.To modify configuration options:
- Open theFactoryTalkAdministration Console and then log on to theFactoryTalk Local Directory.
- ExpandSystem > Policies > Product Policies > Batch > Equipment Editor > Configuration.
- Right-clickOptionsand then selectProperties.
- From theOptions Propertiesdialog box, configure the policy settings and then selectOK.TIP:Restart allFactoryTalk Batchcomponents to update changes made in theFactoryTalk Directory.
Provide Feedback