Equipment and Recipe Editor security
Security for
FactoryTalk Batch Equipment Editor
and FactoryTalk Batch Recipe Editor
is implemented using the FactoryTalk
Security product policies defined in the FactoryTalk
Network Directory. There are two product policy options available:- Access Modesgoverns access to the editors (onlyFactoryTalkusers can be granted access). There are two levels of working access to area models inFactoryTalk Batch Equipment Editor, and recipes inFactoryTalk Batch Recipe Editor.
- View Onlyprovides full viewing privileges, but no changes can be saved.
- Full Editprovides full editing privileges.
- Feature Securitygoverns whichFactoryTalkusers can secure area models and recipes to theFactoryTalkNetwork Directory Security Authority Identifier (SAI).
- TheArea Model: Securepolicy governs which users can secure an area model to a particular SAI inFactoryTalk Batch Equipment Editor.
- TheRecipe: Securepolicy governs which users can secure a recipe to a particular SAI inFactoryTalk Batch Recipe Editor.
Additionally, there are other
Configuration Options
product policies created in the
FactoryTalk
Local Directory for the editors. - To tighten security, remove theAll Usersgroup fromFactoryTalk Batch Equipment EditorandFactoryTalk Batch Recipe Editorproduct policies in theFactoryTalk Directory.
- FactoryTalk Batch Equipment EditorandFactoryTalk Batch Recipe Editorsupport the use of an external security device, such as a retinal scanner.
- In addition toFactoryTalkSecurity, configure Windows security onFactoryTalk Batch Equipment EditorandFactoryTalk Batch Recipe Editorfiles and folders in Windows Explorer.
- RDB security can also be configured when using RDB recipes that are stored inSQL Server®.
Provide Feedback