General usage signature requests
Handling of general usage signature requests
The following explains how general usage signature requests are handled by the
FactoryTalk® Batch
Server:General Usage Signatures | |
|---|---|
Batch Server | General usage signatures are generated by Phase Logic requests
received from Equipment Phases. The equipment phase specifies the
Signature Template ID from which the Signature is generated, and the
Phase Logic Request is considered complete when the Signature
Request is complete. |
Response | If a Phase Logic Request for a General Usage Signature specifies an
invalid Signature Template ID, then the Phase Logic Request is
handled according to standard Phase Logic Request failure protocols.
If the request is successful in generating the Signature, then no
response is made until the Signature is either complete or
cancelled. |
Completion | When the Signature for a General Usage Signature generated by a Phase
Logic Request is complete, then the Phase Logic Request is
considered complete. The Phase Logic Request completion is handled
via the standard Phase Logic Request communication protocol. |
Cancellation | When the Signature for a General Usage Signature generated by a Phase
Logic request is cancelled, the Phase Logic request is considered
failed. The Phase Logic request failure is handled via the standard
Phase Logic request communication protocol. |
Overlap | The Phase Logic Request protocol does not support overlapped Phase
Logic requests; hence, overlapped general usage signatures are not
an issue. Note that parallel recipe phases can create parallel
requests, but no parallelism is possible from within the scope of a
single equipment phase. |
Automatic Cancellation | If the Phase Logic request from which a general usage signature is
generated is aborted, then the general usage signature is System
Cancelled if it is in the incomplete state. |
Warm Restart, Warm All Restart, or Hot Restart | Signature requests generated in response to a General Usage Signature
Phase Logic request are System Cancelled in the event of a
FactoryTalk Batch Server Warm Restart, Warm All Restart, or Hot
Restart. |
Provide Feedback