General usage phase logic requests

A
General Usage Signature
request is created when a General Usage Phase Logic request is sent to the
FactoryTalk Batch
Server during the execution of an automated phase. Each signature template configured in
FactoryTalk Batch Equipment Editor
has a unique template index. To generate a signature the Phase Logic request specifies the signature template index.
For information on configuring general usage phase logic requests, see
Download Batch Parameters
in the .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal