Encoder Configuration view

Use
Encoder Configuration
to define these controller behaviors:
  • Set monitor input voltage.
  • Enable position scaling and endless shaft functionality.
  • Set the numerator and denominator for endless shaft functionality.
  • Set the number of counts per revolution and number of turns.
  • Set the direction of the count.
  • Set the velocity units.
  • Configure velocity filter options.
  • Configure acceleration filter options.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal