Device definition - Events view parameters

The
Events
view in
Device definition
includes these parameters:
Parameter
Description
User Defined Data
Additional data to include when an event occurs. Define up to three instances per event.
Available options are:
  • No Additional Data
  • Stored Count
  • Scaled Count
  • Scaled Stored Count
  • Frequency
  • Average Frequency
  • Stored Frequency
  • Scaled Frequency
  • Scaled Average Frequency
  • Scaled Stored Frequency
  • Pulse Width
  • Average Pulse Width
  • Stored Pulse Width
  • Acceleration
  • Average Acceleration
  • Count
  • Revolution Count
  • Stored Revolution Count
  • Stored Acceleration
  • Scaled Stored Acceleration
  • Scaled Acceleration Average
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal