Device definition - Events view

In
Device definition,
use the
Events
view to configure the user-defined data to include when an event occurs on the device.
To configure event definition parameters, make sure that
Connection
is set to
Data with Events
or
Listen Only with Events
.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal