Configure sourcing output parameters

Configure sourcing output parameters for the output device.
Prerequisites
  • Make sure that
    Output Mode
    is set to
    Sourcing
    .
To configure sourcing output parameters
  1. On the tab for the device, select
    Points
    .
  2. In the
    Points
    view, configure the following parameters as needed:
    • Point Mode
      . Select the operation mode for the point.
    • Enable No Load Detection
      . If applicable, select or clear the checkbox for the point.
    • Diagnostics
      . If online, select diagnostic-icon to view diagnostic information.
    • Output Error Latch Time
      . Enter the time that the error is held to make sure the controller can detect the error and provide more accurate diagnostics.
  3. Select
    OK
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal